|
(Read-Write) Set and query the enumerated value that FieldFox should use to encode the IQ streaming data (e.g., VITA 49A). See also, IQST:DPOR, IQSTR:SRAT, IQST:STAR, IQST:STOP, IQST:DHOS, IQST:SPP, IQST:VITA:MRES, IQST:VITA:MRIP, IQST:VITA:SID,and MEAS:IQAN. Note: 1) FieldFox uses 32-bit IEEE 754 float. 2) Data for the protocols is 2 floating point values per sample (I and Q). |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<enum> |
Enter the streaming protocol for encoding data: VITa49 - sets VITa 49A as the method of encoding the IQ streaming data. DECodio- sets DECodio as the method of encoding the IQ streaming data. DIFi - sets DIFi as the method of encoding the IQ streaming data. |
|
Examples |
IQST:PROT VIT 'Defines VITA 49A as the IQ streaming encoding process for the data |
|
Query Syntax |
IQST:PROT? |
|
Return Type |
enum |
|
Default |
VIT (VITA 49A) |
Last Modified:
|
14Sep2026 |
Add new enum value DIFi for D-series Models (Fluyt) and above |
|
05apr2021 |
New command (A.12.3x) |