|
(Read-Write) Set and query the sample rate for IQ Streaming. If not set, default is AUTO which will sample at 1.25*frequency span. An equivalent setup would be to use: FREQ:SPAN spanValue. See also, IQST:DHOS, IQST:PROT, IQST:SPP, IQST:VITA:MRES, IQST:VITA:MRIP, IQST:VITA:SID, IQST:STOP, IQST:STAR,and MEAS:IQAN. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<float> |
Enter sample rate for IQ streaming. |
|
Examples |
IQST:SRAT 1e6 'Defines the sample rate to 1 MHz for IQ streaming |
|
Query Syntax |
IQST:SRAT? |
|
Return Type |
float |
|
Default |
1.25000000000000E+06 |
Last Modified:
|
05apr2021 |
New command (A.12.3x) |