[:SENSe]:IQSTream:VITA:SIDentifier <int>

(Read-Write) Set and query the stream identifier for this data stream when using the VITA / DIFI protocol.

See also, IQST:DHOS, IQST:SRAT, IQSTR:STAR, IQST:STOP, IQST:PROT,  IQST:SPP, IQST:VITA:DPOR, IQST:VITA:MRIP, IQST:VITA:MRES,and MEAS:IQAN

NOTE: Only VITA protocol 49A is compatible with this command.

Relevant Modes

SA mode (IQ Streaming)

Parameters

 

<int>

The integer value of the VITA identifier.

Examples

IQST:VITA:SID 67 'Sets the stream identifier to protocol 67 (This standard defines a transport-layer protocol designed to promote interoperability between RF (radio frequency) receivers and signal processing equipment in a wide range of applications.)

Query Syntax

IQST:VITA:SID?

Return Type

int

Default

n/a


Last Modified:

05apr2021

New command (A.12.3x)