[:SENSe]:IQSTream:DPORt <int>

(Read-Write) Set and query the destination port (process) to send UDP network packets. E.g., 4991.

See also, IQST:DHOS, IQST:SRAT, IQST:STARt, IQST:STOP, IQST:PROT,  IQST:SPP, IQST:VITA:MRES, IQST:VITA:MRIP, IQST:VITA:SID,and MEAS:IQAN.

NOTE: FieldFox does not support TCP networking.

Relevant Modes

SA

Parameters

 

<int>

Enter destination networking port (process) for the IQ streaming data packets.

Examples

IQST:DPOR 4991 'Defines the destination port (process) to send UDP network packets

Query Syntax

IQST:DPOR?

Return Type

integer

Default

4991

Last Modified:

05apr2021

New command (A.12.3x)