|
(Read-Write) Set and query for VITA / DIFI protocol, the metadata resend interval in packets. A metadata packet will be sent every N data packets for the value of N set here. 0 to disable. See also, IQST:DHOS, IQSTR:SRAT, IQSTR:STARt, IQSTR:STOP, IQST:PROT, IQST:SPP, IQST:VITA:MRES, IQST:VITA:DPOR, IQST:VITA:SID,and MEAS:IQAN. Note: Streaming is used by configuring the desired setup and then starting the acquisition/data stream. In order to make measurement changes (bandwidth, center frequency, etcetera) streaming must be stopped, the new setup configured, and then streaming restarted. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<int> |
Enter a value N that sets the number of data packets for the VITA / DIFI IQ streaming data. 0 to disbale |
|
Examples |
IQST:VITA:MRIP 713 'Sets the value of N data packets to 713 |
|
Query Syntax |
IQST:VITA:MRIP? |
|
Return Type |
integer |
|
Default |
0 |
Last Modified:
|
05apr2021 |
New command (A.12.3x) |