|
(Read-Write) Set and query the number of samples to put in each network packet. The default value of 0 means ‘auto’. If set manually (and too low for the set bandwidth), FieldFox’s network speed may not keep up with the data rate. See also, IQST:DHOS, IQST:SRAT, IQST:STARt, IQST:STOP, IQST:PROT, IQST:DPOR, IQST:VITA:MRES, IQST:VITA:MRIP, IQST:VITA:SID,and MEAS:IQAN. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<int> |
Enter the number of samples to put in each network packet. Auto (0) - In auto mode, packet size increases as bandwidth goes up to achieve more efficiency. Manual (≥1) - Enables you to choose the number of samples to put in each network packet. When set to manual (and if settings is too low for the set bandwidth), FieldFox’s network speed may not keep up with the data rate. |
|
Examples |
IQST:SPP 0'Defines the samples to put in each network packet as auto (the FieldFox decides based on other settings the optimum sample rate to use. |
|
Query Syntax |
IQST:SPP? |
|
Return Type |
int |
|
Default |
0 (Auto) |
Last Modified:
|
05apr2021 |
New command (A.12.3x) |