[:SENSe]:IQSTream:VITA:MRESend

(Write Only) Command only, no argument to re-send the metadata. When in VITA / DIFI streaming mode, causes FieldFox to send a metadata packet containing center frequency, bandwidth, sample rate, etc.

See also, IQST:DHOS, IQST:SRAT, IQST:STAR, IQST:STOP, IQST:PROT,  IQST:SPP, IQST:VITA:DPOR, IQST:VITA:MRIP, IQST:VITA:SID,and MEAS:IQAN

Note: Streaming is used by configuring the desired setup and then starting the acquisition/data stream. In order to make measurement changes (bandwidth, center frequency, etcetera) streaming must be stopped, the new setup configured, and then streaming restarted.

Relevant Modes

SA

Parameters

 

   

Examples

IQST:VITA:MRES */Re-sends the metadata

Query Syntax

n/a

Return Type

n/a

Default

n/a


Last Modified:

05apr2021

New command (A.12.3x)