Frequency
| Offset
| Power
| ALC
| Recvr
Lvl | Source
Ports| #
Points | Trigger
:Ext
Sweep settings:..Time
| Setup
| Segment
| Power |
Phase
| Pulse
Setup | DC
Sources |
Multi-Dimensional Sweep
New See Remotely Specifying a Source Port .
Description |
SCPI |
COM |
|---|---|---|
Start Freq |
||
Stop Freq |
||
Center Freq |
||
Span |
||
CW Frequency |
||
Number of Points |
||
Step size |
||
Freq Offset ON/Off |
||
Read available ranges |
|
|
Read number of ranges |
||
X-Axis display range |
||
Read range name |
||
Read range number |
||
Set range coupling |
||
Set sweep type |
||
Set CW freq |
||
Set start freq |
||
Set stop freq |
||
Set offset value |
||
Set divisor value |
||
Set multiplier value |
||
Freq. Offset Segment Sweep |
||
ON|OFF |
||
Add a segment |
||
Delete a segment |
||
Count the segments |
||
Center Frequency |
||
Frequency Span |
||
Start Frequency |
||
Stop Frequency |
||
Number of Points |
||
IF Bandwidth value |
||
IF Bandwidth control |
||
Source Power value |
||
Source Power control |
||
Sweep time value |
||
Sweep time control |
||
Test Set Switch |
||
Power Settings See Remotely Specifying a Source Port . |
||
Power ON | OFF |
||
Source Power (Auto | ON | OFF) |
||
Power Value |
||
Port Selection |
||
Couple Ports OFF | ON |
||
Attenuator Mode Auto|Manual |
||
Attenuation Value |
||
Power Slope ON | OFF |
||
Power Slope Value |
||
Receiver Attenuation |
||
Set power limit |
||
Power limit ON/OFF |
||
Power limit UI lock |
||
Set offset value |
||
Rx Level ON|OFF |
||
Select the reference receiver |
||
Set maximum iterations |
||
Set tolerance |
||
Set offset value |
||
Separate IFBW |
||
Set Rx IFBW |
||
Safe mode ON|OFF |
||
Safe mode Max power |
||
Safe mode Min power |
||
Use Last Result for Source Power Cal |
||
Returns list of valid ALC Leveling Modes |
||
Set ALC Mode |
||
Sets and returns ALC mode that the Pulse Setup will use when the pulse is turned off |
||
Specifying Source Ports See Remotely Specifying a Source Port. |
||
Returns the number of source ports. |
None |
|
Returns the string names of source ports. |
||
Returns the source port number of the specified string port name. |
None |
|
IF Bandwidth |
||
Previous IF Bandwidth |
None |
|
Next IFBandwidth |
None |
|
Reduce IF BW |
||
Sweep Time Value |
||
Number of Points |
||
Sweep Type (Lin | Pwr | CW | Seg | Phase) |
||
Sweep Generation (Stepped | Analog) |
||
Dwell Time Value |
||
Dwell Time Auto set the minimum dwell time |
||
Sweep Delay |
||
Alternate Sweeps |
||
External ALC |
||
Enable Point Sweep |
||
Fast Sweep |
||
Fast CW |
||
Start Power |
||
Stop Power |
||
Center |
|
|
Span |
|
|
ON|OFF |
||
Add a segment |
||
Delete a segment |
||
Delete all segments |
None |
|
Count the segments |
||
Read the segment number |
None |
|
Segment Center Frequency |
||
Segment Frequency Span |
||
Segment Start Frequency |
||
Segment Stop Frequency |
||
Number of Points |
||
IF Bandwidth |
||
IF Bandwidth Option |
||
Source Power |
||
Source Power Option |
||
X-Axis Point Spacing |
||
Allow Arbitrary Segments |
||
Upload a segment table |
||
Download a segment table |
||
Phase Sweep type |
||
Set fixed phase value |
||
Phase sweep start value |
||
Phase sweep stop value |
||
Phase parameter |
||
Set Phase control mode |
||
Set reference port |
||
Read available phase control modes for the port |
||
Couple sweep settings |
||
Set number of sweep iterations |
||
Set sweep tolerance |
||
Set and read an array of phase offsets. |
||
Use phase offset array. |
||
Set and read an array of ratioed power offsets. |
||
Use power offset array. |
||
Set the fixed power ratioed value |
||
Set the start power ratioed value. |
||
Set the stop power ratioed value. |
||
|
Source (where trigger comes from) |
||
Source (Int | Ext | Manual) |
||
Internal | Manual |
|
|
Trigger! (for Manual Source) |
||
Scope (what is triggered) |
||
Scope (Global | Channel) |
||
Channel Settings (how the channel responds to triggers) |
||
Continuous |
||
Read Continuous Mode |
None |
|
Number of Groups |
||
Read Groups |
None |
|
Hold |
||
Hold Mode (read-only) |
None |
|
All channels in Hold |
||
All channels Resume |
||
Single |
||
Trigger Mode (Channel | Point | Sweep) |
||
Restart |
|
|
Abort |
||
Scope (Global/Chan) |
||
Trigger Delay (Global) |
||
Trigger Delay (Channel) |
||
MeasTrigIn/ Hand I/O |
||
Level or Edge |
||
Neg/Low or Pos/High |
||
Accept Trigger Before Armed |
||
Ready for Trigger Indicator (Out) |
||
MeasTrig Rdy/ Hand I/O |
|
|
Checks if the PNA is ready for a hardware trigger |
||
High / Low |
||
Which AuxTrig connector pair being used. |
N/A |
|
How many Aux connector pairs. |
||
AUX TRIG OUT |
||
Enable |
||
Global or Channel Pref. |
||
Polarity (Pos/Neg) |
||
Position (Before/After acq) |
||
OUT Pulse width |
||
Point or Sweep. |
||
AUX TRIG (Ready) IN |
|
|
Enable Handshake |
||
Edge or Level Level NOT in UI. |
||
Polarity High/leading or Low/trailing. |
||
Delay |
||
Pulse Meas Mode |
||
Autodetect Pulse mode |
||
Set Pulse Mode (Narrow | Wide) |
||
Autoselect IFBW |
||
Autoselect IF Gain |
||
Autoselect Pulse clock period |
||
Autoselect Width and Delay |
||
Autoselect Pulse Gens |
||
Autoselect CW Sweep Time |
||
Pulse (manual) Settings |
SCPI |
COM |
|---|---|---|
Set master pulse frequency |
||
Set master pulse period |
||
Set master pulse width |
Enable Pulse output ON | OFF |
||
Set Pulse Period for ALL pulse generators |
||
Set Pulse Delay |
||
Set Pulse Width |
||
Set Pulse delay increment |
||
Enables Subpoint triggering |
||
Set Pulse Invert |
||
Internal Pulse Modulator Enable |
||
PulseSyncIn Trigger Polarity |
||
PulseSyncIn Trigger Type |
||
Sync receiver to Pulse0 (enable pulse0) |
||
Pulse Trigger Source |
||
SCPI |
COM |
|
|---|---|---|
Source names catalog |
||
Enable source outputs |
||
Source state |
||
Start DC |
||
Stop DC |
||
Data |
||
Set and return the Max DC limit value for a DC source |
||
Set and return the Min DC limit value for a DC source |
Set and read the order for the specified DC source in the multi-dimensional sweep. |
||
Set and read the specified DC source’s ON/OFF state in the multi-dimensional sweep. |
||
Read the names of source domains in the multi-dimensional sweep whose state is ON and whose dimension order is the specified dimension order. |
||
Read the highest dimension order in the multi-dimensional sweep. |
||
Set and read the point count for the specified dimension order in the multi-dimensional sweep. |
||
Set and read the repeat count for the specified dimension order in the multi-dimensional sweep. |
||
Set and read the source frequency domain’s order in the multi-dimensional sweep. |
||
Set and read the source frequency domain’s ON/OFF state in the multi-dimensional sweep. |
||
Set and read the fixed frequency value for a specific port. |
||
Set and read the start frequency value for a specific port. |
||
Set and read the stop frequency value for a specific port. |
||
Set and read the source phase domain’s order in the multi-dimensional sweep. |
||
Set and read the source phase domain’s ON/OFF state in the multi-dimensional sweep. |
||
Set and read the source power domain’s order in the multi-dimensional sweep. |
||
Set and read the source power domain’s ON/OFF state in the multi-dimensional sweep. |
||
![]()