Set up your measurement using the following information:
Preset the Analyzer
Measurement Classes
Select a Measurement Parameter
Set Frequency Range
Set Power Level
Set Sweep Type
Set Number of Points
Set Triggering
Set Data Format
Set Scale
Pre-configured Measurement Setups
Customize the Screen
Undo/Redo Settings
Source Phase Control (Opt 088)
Phase Coherent Measurements
Receiver Leveling
ADC Measurements
Copy Channels
RF Path Configurator
Caution: Avoid expensive repairs to your analyzer. Read Electrostatic Discharge Protection.