:ACQuire:COUNt
Command Syntax
:ACQuire:COUNt <count>
<count> is an int.
Query Syntax
:ACQuire:COUNt?
Description
When the AVERage acquisition sampling mode is selected (see :ACQuire:SMODe), this command specifies the number of waveforms/acquisitions to average to give the averaged waveform result. You can enter a value between 2 and 1M. The default value for the number of averages is 16.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.