:ACQuire:POINts
Command Syntax
:ACQuire:POINts <memory_depth>
<memory_depth> is a double.
Query Syntax
:ACQuire:POINts?
Description
When :ACQuire:POINts:AUTO OFF, the command lets you manually specify the acquisition memory depth in points (pts).
Whether the :ACQuire:POINts:AUTO is OFF or ON, the query returns the memory depth that has been manually set or automatically determined.
Using the :MAXimum? Common Child Query to Find Oscilloscope Hardware Limits
The :MAXimum? common child query (see Common Child Commands) can be used to determine the oscilloscope's, possibly licensed, hardware capabilities.
For example, after sending the :ACQuire:POINts:AUTO OFF command and making a single acquisition (:ACQuire:SINGle), the :ACQuire:POINts:MAXimum? query will tell you the oscilloscope maximum memory depth.