:ACQuire:SRATe:AUTO

Command Syntax

:ACQuire:SRATe:AUTO {OFF | ON}

Query Syntax

:ACQuire:SRATe:AUTO?

Description

When ON, the sample rate is automatically determined based on the timebase and memory depth settings so that waveform data will fill the display.

When OFF, you manually specify the sample rate using the :ACQuire:SRATe command.

The query returns the currently specified setting.