:ACQuire:SRATe
Command Syntax
:ACQuire:SRATe <sample_rate>
<sample_rate> is a double.
Query Syntax
:ACQuire:SRATe?
Description
When :ACQuire:SRATe:AUTO OFF, the command lets you manually specify the acquisition sample rate in samples per second (Sa/s).
Whether the :ACQuire:SRATe:AUTO is OFF or ON, the query returns the sample rate that has been manually set or automatically determined.