:ACQuire:STOP

Command Syntax

:ACQuire:STOP

Description

Stops data acquisition. This command is equivalent to clicking the Stop button. This command does not erase display memory. To clear display memory, use the :ACQuire:CDISplay command. Use the :ACQuire:RUN command to resume data acquisition. When acquisition is stopped, use the :ACQuire:SINGle command to start a single run of capturing waveform data.