:ACQuire:POINts:AUTO

Command Syntax

:ACQuire:POINts:AUTO {OFF | ON}

Query Syntax

:ACQuire:POINts:AUTO?

Description

When ON, the memory depth is automatically determined based on the timebase and sample rate settings so that waveform data will fill the display.

When OFF, you manually specify the memory depth using the :ACQuire:POINts command.

The query returns the currently specified setting.