:CGMemory:CWINdow

Command Syntax

:CGMemoryN:CWINdow TIME{1:4}

Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Query Syntax

:CGMemoryN:CWINdow?

Description

The :CGMemory{1:8}:CWINdow command allows you to assign a color grade memory waveform to a Waveform content window.

Command Arguments and Content Windows
Argument Displayed Waveform
Content Window
Number of
Available Windows
Scale Units
Programmatically Via
Front Panel
TIME{1:4} Waveform 4 4 Y-Axis: Volts or Watts (linear scale)
X-Axis: seconds