:CGMemory:DSTatus?
Query Syntax
:CGMemoryN:DSTatus?
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Response
{CORR | INV}
Description
Returns the status of the specified waveform memory. Up to eight memories are available. To query the reason for the current state of the memory, use the :CGMemory:DSTatus:REASon? query. The following responses can be returned:
CORR- The color grade memory location contains eye waveform data. To clear memory, use the
:CGMemory:CLEarcommand. INV- The color grade memory location does not contain waveform data.