:CGMemory:DSTatus:DETails?
Query Syntax
:CGMemoryN:DSTatus:DETails?
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Response
<string>
Description
If the status of the color grade/gray scale memory is questionable or invalid (see :CGMemory:DSTatus?), this query returns a string that may provide additional details.
If the status of the color grade/gray scale memory is valid, this query returns an empty string.
For a basic reason for the questionable or invalid status, use the :CGMemory:DSTatus:REASon? sibling query.