:CGMemory:UNAMe
Command Syntax
:CGMemoryN:UNAMe <string>
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Query Syntax
:CGMemoryN:UNAMe?
Description
Assigns a custom user name to an eye-memory waveform. User names are helpful because they identify what a waveform represents rather than the oscilloscope's input channel. For example, you could assign user name "DUT Output" to the memory 2 waveform. User names can be 25 characters or less and are displayed on the screen and on screen captures. To remove a custom user name, re-create it using an empty string. To assign the user name to the name of the gray-scale and color-grade database waveform file that was imported into color grade memory, use the :CGMemory:UNAMe:UFName command.
Custom user names can by created for other waveforms using the following commands:
Example Command Sequence
:CGMemory2:UNAMe "DUT Output"