:CGMemory:UNAMe:UFName
Command Syntax
:CGMemoryN:UNAMe:UFName
Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.
Description
Automatically sets the gray-scale/color-grade memory's user name to the name of the waveform's source file. If the waveform was loaded from a displayed input channel, the name of the file that was automatically created when the data was loaded is used. To learn about user names, use the default user name, or enter a custom user name, use the :CGMemory:UNAMe command.