:CGMemory:STATus?

Query Syntax

:CGMemoryN:STATus?

Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Query Response

{AVA | UNAV}

Description

Queries the availability of color grade memory for use. Color grade memory becomes available (AVA) after data has been loaded into memory using the :CGMemory:FILE:LOAD command. Color grade memory does not need to be displayed to be classed as available. Color grade memory is unavailable (UNAV) if data has not been loaded into the memory.

Use the :CGMemory:DISPlay command query to determine if a Color grade memory waveform is displayed.