:CGMemory:DSTatus:REASon?

Query Syntax

:CGMemoryN:DSTatus:REASon?

Where N identifies one of eight color grade memories. For example, the color grade memory 2 would be identified as :CGMemory2.

Query Response

<string>

Description

Returns a description of the status of the specified color grade memory. If an eye waveform is currently in the specified color grade memory location, the name of the source waveform will be returned. For example, "Source: Channel 1_1". If the color grade memory is empty, the string "Please select a file." is returned. If the file is corrupt or an incorrect type, the string "Unable to load file." is returned. To check the status of the color grade memory, use the :CGMemory:DSTatus? parent query.