:DIFF:EYE:CCOunt

Command Syntax

:DIFFN:EYE:CCOunt <num_hits>
            

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

<num_hits> is an integer.

Query Syntax

:DIFFN:EYE:CCOunt?

Description

This command specifies the minimum highest hit count in the real-time eye's color grade - gray scale database that must occur before making measurements on the data. Increasing this value lets more waveforms be collected before making measurements, thereby increasing measurement accuracy. The default value for this control is 1.