:DIFF:EYE:XPOSition

Command Syntax

:DIFFN:EYE:XPOSition <time>
            

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

<time> is a double.

Query Syntax

:DIFFN:EYE:XPOSition?

Description

Sets the differential waveform N horizontal time position (center display location) of the real-time eye display.

This command directly affects the real-time eye's horizontal position setting in UI (unit interval) units (see the :DIFF:EYE:UIXPosition command).

To set the horizontal time scale of the real-time eye display in seconds-per-division, use the :DIFF:EYE:XSCale command.