:DIFF:EYE:UIXPosition
Command Syntax
:DIFFN:EYE:UIXPosition <time_in_UI>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<time_in_UI> is a double in UI (unit interval) units.
Query Syntax
:DIFFN:EYE:UIXPosition?
Description
Sets the differential waveform N horizontal time position (center display location) of the real-time eye display in UI units.
This command directly affects the real-time eye's horizontal position setting in seconds (see the :DIFF:EYE:XPOSition command).
To set the horizontal time range of the real-time eye display in UI units, use the :DIFF:EYE:UIXRange command.