:DIFF:EYE:XSCale
Command Syntax
:DIFFN:EYE:XSCale <seconds_per_div>
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
<seconds_per_div> is a double.
Query Syntax
:DIFFN:EYE:XSCale?
Description
Sets the differential waveform N horizontal time scale of the real-time eye display in seconds-per-division.
This command directly affects the real-time eye's horizontal range setting in UI (unit interval) units (see the :DIFF:EYE:UIXRange command).
To set the horizontal position (center display location), use the :DIFF:EYE:XPOSition command.
Only the center UI is valid for the recovered clock edge. You can display up to 10 UIs to show context before and after the center UI.