:DIFF:EYE:UIXRange

Command Syntax

:DIFFN:EYE:UIXRange <time_in_UI>
            

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

<time_in_UI> is a double in UI (unit interval) units.

Query Syntax

:DIFFN:EYE:UIXRange?

Description

Sets the differential waveform N horizontal time range (width) of the real-time eye display in UI units.

This command directly affects the real-time eye's horizontal time/div setting in seconds (see the :DIFF:EYE:XSCale command).

To set the horizontal position (center display location) of the real-time eye display in UI units, use the :DIFF:EYE:UIXPosition command.

Only the center UI is valid for the recovered clock edge. You can display up to 10 UIs to show context before and after the center UI.