:DIFF:SNDRatio:FILE:NAME
Command Syntax
:DIFFN:SNDRatio:FILE:NAME "filename"
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:SNDRatio:FILE:NAME?
Query Response
"string"
Description
When FILE is selected as the SNDR standard (see :DIFF:SNDRatio:STANdard), this command specifies the name of the SNDR standard definition file.
Use the :DIFF:SNDRatio:FILE:RELoad command to reload the SNDR standard definition file, for example, after loading a setup file that has FILE selected as the SNDR standard.