:DIFF:SNDRatio:SAVE
Command Syntax
:DIFFN:SNDRatio:SAVE {OFF | ON}
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:SNDRatio:SAVE?
Description
When AUTomatic is selected as the SNDR standard (see :DIFF:SNDRatio:STANdard), this command lets you turn on or off saving of the automatically calculated Sigma-n locations to a standard definition file.
When saving the automatic calculations to a standards file is turned on, use the :DIFF:SNDRatio:SAVE:FILE command to specify the file name.