:DIFF:SNDRatio:STANdard

Command Syntax

:DIFFN:SNDRatio:STANdard {ASA13 | AUTomatic | PCIe | IDJ | IEEe | ASA45 | USB4 | FILE}

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:SNDRatio:STANdard?

Description

Select the technology standard you want to use for SNDR measurement definitions:

SNDR Standards
Signal Type Standard Notes
NRZ ASA13 ASA SG1-3 (Speed Grade SG1, SG2, or SG3) — This selection uses the technique outlined in the ASA (Automotive SerDes Alliance) Transceiver specification version 1.1 section 4.4.1.1.2.
NRZ, PAM3, PAM4 AUTomatic Based on the input pattern, the algorithm looks for ideal points that can be used to calculate Sigma-n. Any pattern that contains every signal level is supported. Then, the Sigma-e and Pmax measurements are calculated using the same method as IEEe (without requiring the PRBS13Q pattern).
PAM4 PCIe PCIe 6.0 — This selection, available with PAM4 signal types, uses a process described in the PCIe 6.0 standard.
PAM4 IDJ IEEE 802.3 dj — This is the same as the IEEe option except it uses PCIe Sum of Squares of LFPR for "Pmax" instead of just maximum.
PAM4 IEEe IEEE (PRBS13Q) — This selection uses the technique outlined in the IEEE 802.3 specification clause 120D.3.1.6. The algorithm looks for six or more consecutive identical symbols and places the voltage measurement at the center of the 3rd UI. The variance of all those measurements is taken and then the standard deviations are averaged to get σn.

The PRBS13Q pattern provides runs of at least six consecutive identical PAM4 symbols at each of the PAM4 levels.
PAM4 ASA45 ASA SG4, 5 (Speed Grade SG4 or SG5) — This selection uses the technique outlined in the ASA (Automotive SerDes Alliance) Transceiver specification version 1.1 section 4.4.1.1.2.
PAM3 USB4 This selection uses the technique outlined in the USB4 specification version 2.0 section 3.2.3.4.
NRZ, PAM3, PAM4 FILE This selection allows for custom measurement parameters loaded from a file.

The format of this file is proprietary. For help developing custom files, contact Keysight Technical Support and ask for an Application Engineer.

The options available depend on the signal type selection (see :DIFF:SIGNal:TYPE).

When FILE is selected as the SNDR standard, use the :DIFF:SNDRatio:FILE:NAME command to specify the name of the SNDR standard definition file, and use the :DIFF:SNDRatio:FILE:RELoad command to reload the SNDR standard definition file, for example, after loading a setup file.