:DIFF:SNDRatio:RNCValue:LEVel

Command Syntax

:DIFFN:SNDRatio:RNCValue:LEVel{0:3} <custom_RN_value>

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

<custom_RN_value> is a double.

Query Syntax

:DIFFN:SNDRatio:RNCValue:LEVel{0:3}?

Description

When using custom RN compensation (see :DIFF:SNDRatio:RNComp), this command lets you specify the custom RN values for the symbol levels.