:DIFF:SNDRatio:NAVerages
Command Syntax
:DIFFN:SNDRatio:NAVerages <number_of_averages>
<number_of_averages> is an integer.
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:SNDRatio:NAVerages?
Description
Specifies the number of patterns to average in the SNDR linear fit computation.
Technology standard test documents typically tell you the value expected to be used for this parameter.