:FUNCtion:PATTern:FILE:GCODe
Command Syntax
:FUNCtionN:PATTern:FILE:GCODe {ON | OFF | 1 | 0}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:PATTern:FILE:GCODe?
Query Response
{1 | 0}
Description
When you have specified a PAM4 signal type (see :FUNCtion:SIGNal:TYPE), this command lets you specify whether symbols are Gray Coded or uncoded. When patterns are specified (see :FUNCtion:PATTern:FILE:NAME), the pattern must match this selection.