:FUNCtion:PATTern:FILE:RELoad

Command Syntax

:FUNCtionN:PATTern:FILE:RELoad

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Description

When you have specified a PAM signal type (see :FUNCtion:SIGNal:TYPE) and specified the signal pattern by loading a pattern file (see :FUNCtion:PATTern:FILE:NAME), this command reloads the specified pattern file. Reloading is useful when there have been changes to the pattern file that was previously loaded.