:FUNCtion:UNAMe

Command Syntax

:FUNCtionN:UNAMe <string>

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:UNAMe?

Description

Assigns a custom user name to a function waveform. User names are helpful because they identify what a waveform represents rather than the function name. For example, you could assign user name "Transceiver Output" to the memory 2 waveform. User names can be 25 characters or less and are displayed on the screen and on screen captures. To remove a custom user name, re-create it using an empty string.

Custom user names can by created for other waveforms using the following commands:

Example Command Sequence

:FUNCtion2:UNAMe "Transceiver Output"