:FUNCtion:PATTern:TRACking
Command Syntax
:FUNCtionN:PATTern:TRACking {{ON | 1} | {OFF | 0}}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:PATTern:TRACking?
Query Response
{1 | 0}
Description
This command specifies whether the math function has the same pattern as the input waveform.