:FUNCtion:SNOise:SNValue:LEVel{0:3}?
Query Syntax
:FUNCtionN:SNOise:SNValue:LEVel{0:3}?
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Description
This query returns the calibrated oscilloscope noise value at the specified level.
AN NRZ signal has LEVel0 and LEVel1. A PAM3 signal has LEVEL0, LEVel1, and LEVel2. A PAM4 signal has LEVEL0, LEVel1, LEVel2, and LEVel3.
Use the :FUNCtion:SNOise:CALibrate command to start the oscilloscope noise calibration.