:FUNCtion:PATTern:MODE
Command Syntax
:FUNCtionN:PATTern:MODE {ADETect | KPATtern | PFILe}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:PATTern:MODE?
Description
For data measurements like BER/SER (Bit/Symbol Error Ratio) where the measurement must know the pattern of a data signal, this command selects how the pattern is determined:
-
ADETect— (Auto Detect) This option tells the oscilloscope to automatically determine the pattern length and pattern by looking for at least two error-free copies of an identical repeating bit pattern in acquisition memory. -
KPATtern— (Known Pattern) This option lets you select the pattern from a list of known patterns (see:FUNCtion:PATTern:KPATtern). -
PFILe— (Pattern File) This option lets you load a pattern file that tells the oscilloscope the pattern length and pattern to measure against.Use the
:FUNCtion:PATTern:FILE:NAMEcommand to select the pattern file.