:FUNCtion:SNDRatio:FILE:NAME

Command Syntax

:FUNCtionN:SNDRatio:FILE:NAME "filename"

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:SNDRatio:FILE:NAME?

Query Response

"string"

Description

When FILE is selected as the SNDR standard (see :FUNCtion:SNDRatio:STANdard), this command specifies the name of the SNDR standard definition file.

Use the :FUNCtion:SNDRatio:FILE:RELoad command to reload the SNDR standard definition file, for example, after loading a setup file that has FILE selected as the SNDR standard.