:FUNCtion:SNDRatio:RNComp

Command Syntax

:FUNCtionN:SNDRatio:RNComp {OFF | AUTomatic | CUSTom}

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:SNDRatio:RNComp?

Description

This command disable disables RN compensation (OFF), enables compensation for oscilloscope RN (AUTomatic), or enables user-defined values for RN compensation (CUSTom).

If there are known contributors to random noise, you can use RN Compensation to compensate or remove noise from the measurement results.

When CUSTom is selected, use the :FUNCtion:SNDRatio:RNCValue:LEVel command to specify the appropriate RN compensation values for the symbol levels.