:FUNCtion:SNDRatio:NAVerages
Command Syntax
:FUNCtionN:SNDRatio:NAVerages <number_of_averages>
<number_of_averages> is an integer.
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:SNDRatio:NAVerages?
Description
Specifies the number of patterns to average in the SNDR linear fit computation.
Technology standard test documents typically tell you the value expected to be used for this parameter.