:FUNCtion:SNDRatio:FILE:RELoad

Command Syntax

:FUNCtionN:SNDRatio:FILE:RELoad

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Description

When FILE is selected as the SNDR standard (see :FUNCtion:SNDRatio:STANdard) and the file name has been specified (see :FUNCtion:SNDRatio:FILE:NAME), this command reloads the SNDR standard definition file, for example, after loading a setup file.