:FUNCtion:SNDRatio:RNCValue:LEVel

Command Syntax

:FUNCtionN:SNDRatio:RNCValue:LEVel{0:3} <custom_RN_value>

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

<custom_RN_value> is a double.

Query Syntax

:FUNCtionN:SNDRatio:RNCValue:LEVel{0:3}?

Description

When using custom RN compensation (see :FUNCtion:SNDRatio:RNComp), this command lets you specify the custom RN values for the symbol levels.