:FUNCtion:SNDRatio:SAVE

Command Syntax

:FUNCtionN:SNDRatio:SAVE {OFF | ON}

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:SNDRatio:SAVE?

Description

When AUTomatic is selected as the SNDR standard (see :FUNCtion:SNDRatio:STANdard), this command lets you turn on or off saving of the automatically calculated Sigma-n locations to a standard definition file.

When saving the automatic calculations to a standards file is turned on, use the :FUNCtion:SNDRatio:SAVE:FILE command to specify the file name.