:FUNCtion:SNDRatio:LFPDelay
Command Syntax
:FUNCtionN:SNDRatio:LFPDelay <number_of_UIs>
<number_of_UIs> is an integer.
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:SNDRatio:LFPDelay?
Description
This parameter is used in the filter to compute the linear fit pulse response. It is also a number of unit intervals (UIs). It is sometimes denoted using Dp.
Technology standard test documents typically tell you the value expected to be used for this parameter.