:FUNCtion:STATus?
Query Syntax
:FUNCtionN:STATus?
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Response
{AVA | UNAV}
Description
Queries the availability of a math function for use. A math function becomes available (AVA) after the function is defined using the :FUNCtion:FOPerator command. The math function does not need to be displayed to be classed as available. Available math functions are shown in the Signals Palette. A math function is unavailable (UNAV) if a function has not been created.
Use the :FUNCtion:DISPlay command query to determine if a math function output waveform is displayed.