:FUNCtion:XPOSition

Command Syntax

:FUNCtionN:XPOSition   <time>

<time> is a double.

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:XPOSition?

Description

Sets the horizontal time position. The horizontal position is the time delay relative to the trigger event, which is referenced to the display's left edge or center (:FUNCtion:XREFerence?).