:FUNCtion:YSCale
Command Syntax
:FUNCtionN:YSCale <amplitude>
<amplitude> is a double.
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:YSCale?
Description
Sets the vertical scale (sensitivity). This is volts-per-division for electrical waveforms and watts-per-division for optical waveforms. Vertical scaling (:FUNCtion:VERTical:SCALing) automatically changes the mode from auto to manual. The vertical expansion and contraction is about the center offset value (:FUNCtion:YOFFset). For optical channels, vertical expansion and contraction is about the second graticule division from the bottom of the display screen and also not at the ground reference.