:FUNCtion:XSCale:FINE
Command Syntax
:FUNCtionN:XSCale:FINE {{OFF | 0} | {ON | 1}}
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:XSCale:FINE?
Query Response
{0 | 1}
Description
Enables or disables fine adjustment of the horizontal scale.
When OFF (coarse adjustment), the horizontal scale is adjusted in a 1-2-5 sequence.
When ON (fine adjustment), the horizontal scale is adjusted in smaller, evenly spaced increments.