:FUNCtion:YSCale:FINE

Command Syntax

:FUNCtionN:YSCale:FINE {{OFF | 0} | {ON | 1}}

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Query Syntax

:FUNCtionN:YSCale:FINE?

Query Response

{0 | 1}

Description

Enables or disables fine adjustment of the vertical scale.

When OFF (coarse adjustment), the vertical scale is adjusted in a 1-2-5 sequence.

When ON (fine adjustment), the vertical scale is adjusted in smaller, evenly spaced increments.